¿Cómo podemos ayudarte hoy?

What replaces the CAT6-POE (ASCO 185)?

Issue:

Replacement for old ASCO 185 CAT6-POE

Product Line:

Surge Protection Device

Answer:

The CAT6-POE (ASCO 185) crosses to the SSP057POESE10IG.

Similar to this is the RM-CAT6-POE (ASCO 186) which is still active in the 8-channel version (186D068S10KX08N0). If you need to protect more than 8 channels, you can purchase the added module RM-CAT6-MOD1 that will protect an additional 8 channels. You can add this modules for every 8 channels they want to protect.