¿Cómo podemos ayudarte hoy?

Is HVMB305200 available in NEMA 12 enclosure?

Issue:

Is HVMB305200 rated NEMA 12?

Product Line:

Switchboards/Switchgears

Answer:

HVMB305200 is NEMA 1 or NEMA 3R rated only. We do not offer it in NEMA 12.

Schneider Electric Mexico