What terminations are available for the HC2SN Neutral Assembly for I-line interiors
Issue:
Termination/Wire Size
Product Line:
Panelboards
Environment:
I-Line
Cause:
Installation
Resolution:
Main Lug Terminals : (2) #6-300kcmil Al or Cu
(2) Bar A: (34) #4 - 14 AWG Al or Cu (Each Bar A = 17 terminations.)
(1) Bar B: (11) #14 - #4 Al or Cu
(1) Bar C: (9) #14 - 1/0 AWG Al or Cu
Termination/Wire Size
Product Line:
Panelboards
Environment:
I-Line
Cause:
Installation
Resolution:
Main Lug Terminals : (2) #6-300kcmil Al or Cu
(2) Bar A: (34) #4 - 14 AWG Al or Cu (Each Bar A = 17 terminations.)
(1) Bar B: (11) #14 - #4 Al or Cu
(1) Bar C: (9) #14 - 1/0 AWG Al or Cu
Publicado para: Schneider Electric Mexico