¿Cómo podemos ayudarte hoy?

What's the trench duct 12" to 9" right hand reducer part number?

Issue:

Looking for 12 to 9 inches tall right hand reducer

Product Line:

Busway and Trench Ducts

Answer:

The catalog number for the 12" to 9" right hand reducer is RRV122100009RR.