What is the difference between MH86BEP and MH86D9?
Issue: Clarification-Product features
Product Line: Panelboards
Resolution: The D9 suffix option is for the box to be made 9" Deep vs the standard 5.75" Deep.
The BE suffix indicates blank endwalls or no knockouts.
The box suffix "P" represents ANSI 49 paint. Standard NEMA 1 MH boxes are not painted.