Are NQ and NF panelboards have MIL-STD-461G rating?
Issue:
MIL rating for panelboards
Product Line:
NQ and NF panelboard
Resolution:
NF and NQ Panelboards are NOT built to Mil Specs. Most NF and NQ Panelboards will be resilient against electromagnetic interference due to two factors:
1) NF and NQ Panelboards are supplied with steel enclosures, which provide considerable protection against EMF.
2) Nearly all the circuit breakers installed in NF and NQ Panelboards have Thermal-Magnetic trip units with no electronic components, therefore are inherently less sensitive to EMF interference than microelectronic circuits.
Publicado para: Schneider Electric Mexico