Is it possible to use a Powerpact L-frame main breaker breaker on an NF SPD panelboard?
Product Line:
NF Panelboard
Environment:
Low Voltage Panelboard
Cause:
Getting an error converting a 400A NF MLO panelboard with integral SPD to Main Breaker style.
Resolution:
The only allowed main breaker to use on a 400A NF panelboard with factory built SPD is the LA/LH frame breaker. Powerpact L-frame is not allowed. If the 400A NF MLO panelboard is already existing, should be able to add a LA/LH main breaker kit to the panelboard in the field.
Publicado para: Schneider Electric Mexico