¿Cómo podemos ayudarte hoy?

Does Schneider offer stainless steel weather shield for stainless steel transformers?

Product Line:

EX/EXN Transformers.

Environment:

Transformers with M style Enclosures.

Cause:

Customer quoting an EXN150T3HSS 304 Stainless transformer and trying to verify if still need to include a weather shield.

Resolution:

All Enclosure M Transformers such as EXNs do not offer stainless steel weather shields due to very few applications where customer requires stainless steel weather shields, Schneider Electric chose to no offer it for the DOE 2016 solution and we have no plans to offer in the future. The EXN NEMA 4X transformers do not offer a weather shield so it does not need to be included.

Schneider Electric Mexico

Explora más
Producto:
Explora más
Producto: