¿Cómo podemos ayudarte hoy?

What Is the difference between PBPEDU5B100FOON530T and PBPEDU5B100FOOL530M1

Issue:

Difference between PBPEDU5B100FOON530T and PBPEDU5B100FOOL530M1

Product Line:

I Line II Busway

Cause:

Product Characteristics

Resolution:

These units are the same except for the following:

PBPEDU5B100FOON530T comes with:

N530 Non-Locking Connector and a carrying handle.

'T' denotes carrying handle

N530 Non-Locking Connector

description 1

PBPEDU5B100FOOL530M1 comes with:

L530 Locking Connector and a 208Y/120V PM5350 Meter.

'M1' denotes factory-installed meter

Locking Connector

description 2

Both of these units are 30A rated and have the 200% neutral (noted by the '5B' in the catalog number.

30A rated and have the 200% neutral