Can a piece, elbow, or flange of I-Line/ I-Line II busway be connected to a different amperage rating piece of I-Line/ I-Line II busway (e.g. connecting a 2500A to a 3000A I-Line II piece of busway)?
Issue:
Connecting a piece of busway to a different amperage rating piece of I-Line/ I-Line II Busway
Product Line:
I-Line, I-Line II Busways
Environment:
Installation
Cause:
Unit compatibility and ordering
Resolution:
The only way to connect the two different ampere ratings I-Line/I-Line II Busways is to use a special unfused reducer. Contact your Square D authorized local distributor to build a custom unfused reducer according to your application.