¿Cómo podemos ayudarte hoy?

What is the required size for Square D transformer sound isolation pads?

Product Line:

Energy Efficient Transformers

Environment:

Low Voltage Transformers

Cause:

Required size (i.e. thickness, width, length) for 300kVA dry type transformers.

Resolution:

Square D / schneider Electric do not have any specified size for sound isolation pads. Details required to mount a transformer in conformance with applicable Code requirements need to be specified by a local structural or civil engineer. The knowledge of a building’s structural components, the features of a building’s locale, and familiarity the Code(s) which apply are the province of the customer’s engineer. The engineer will need to specify the anchoring components, housekeeping/vibration pads and any other components that might be part of the load path which restrains the installed transformer at its hard mounting points.

Our online drawings provide mounting dimensions, mounting hole dimensions, overall dimensions, unit weight and approximate center of gravity location.

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: