What is the catalog number of replacement neutral bonding provisions for 400, 600, and 800 A NF panelboard?
Issue:
To replace existing standard neutral bonding provisions on a 400, 600, and 800 A NF interior
Product Line:
Panelboard
Environment:
NF, 400A, 600A, 800A panel board interior
Resolution:
80113-675-51 is the part number for 400, 600, and 600 A neutral bonding provisions for NF Panelboards. Includes lugs and required screws. Find more replacement parts for NF Panelboards in our 1670DB0802 Data Bulletin.