¿Cómo podemos ayudarte hoy?

Do NQ panels have intermediate supports on the bus bars to prevent deflection?

Product Line:

NQ Panelboard


Environment:

Low Voltage Panelboard interior


Cause:

NQ Panel Bus Bar Deflection


Resolution:

It depends on how many circuits are in the panel. The 42-circuits and below are just supported at each end, the 54-circuit and above would have intermediate supports on the bus bars. Intermediate supports on the bus bars are not offered as special.