¿Cómo podemos ayudarte hoy?

Does Square D / Schneider Electric offer an isolated ground bar for QED Switchboard?

Product Line:

QED-2 Switchboard

Environment:

Switchboard Low Voltage Product.

Cause:

Need isolated ground bar for QED switchboard.

Resolution:

We can provide an Isolated Ground Bar on QED Switchboards. It just needs to be noted on the drawings/specification that IsoGround is required. The way it is assembled is, there is a ground bar, mounted over the normal ground bar with Isolation Standoffs. So basically, just a stacked ground bar system separated by Isolators. For assistance on how to add this feature on Product Selector nor SE Advantage, contact your local Square D field office.