¿Cómo podemos ayudarte hoy?

Is the new MPU style Mini-Powerzone CSA rated?

Product Line:

LV Transformers


Environment:

Applies to Mini Power Zone Transformers from Square D/Schneider Electric


Cause:

Mini Power Zone Transformers are primarily designed and built for use in the USA


Resolution:

No, the Mini Power Zones are UL Listed, and are used primarily in the USA, and that is true of the newer MPU models. CSA is a Canadian standard that the MPZ/U/B units do not conform to.

Schneider Electric Mexico

Explora más
Producto:
Explora más
Producto: