¿Cómo podemos ayudarte hoy?

How to Identify the 9001K Selector Switch Part number?

Issue:

There is no label nor marking for the part number, unable to identify an existing 9001K/SK selector switch

Product Line:

9001K / 9001SK Selector Switches

Environment:

Push Buttons and Operator Interface

Resolution:

1. The important step is to identify the cam code located behind the selector switch head. Please refer to the picture below.

2. The switch features also needs to be determined:

- metal or plastic ring nut

- maintained or momentary

- knob or key

3. Finally, identify the part number from the list in the catalog or Schneider Electric Digest.

9001K selector switch cam

Schneider Electric Mexico

Documentos adjuntos
9001K Selector Switches.pdf [1.2 MB]