¿Cómo podemos ayudarte hoy?

Does the iEM3400 and iEM3500 series meters support High leg Delta wiring?

Issue

Can the iEM3400 and iEM3500 series meters be wired as high leg delta or not?

Product line

iEM3400 and iEM3500

Environment

Application requires the installation of a power meter or replacement existing meter in a high leg delta system.

Resolution

No. These meters (iEM3400 and iEM3500 Series) do not support the electrical system type for High-Leg Delta.

The electrical system types supported, per the User Guide, https://www.se.com/us/en/download/document/7EN02-0438/

3PH3W

3PH4W

1PH2W L-N

1PH2W L-L

1PH3W L-L-N

1PH4W Multi L-N

As an alternative, please look at the PM5000 series for High Leg Delta supported models.  See FAQ FA232893