¿Cómo podemos ayudarte hoy?

EcoStruxure Machine Expert v2.3 is missing J1939

Issue

In EcoStruxure Machine Expert v2.3, it is not possible to add the J1939_Manager node network protocol in the Device Tree.

This is what the node appears like under the CANopen bus in the Device Tree in prior version v2.2.2:

J1939_Manager can be added in Machine Expert v2.2.2 under the CANopen bus node

However, in Machine Expert v2.3, it is no longer seen in the Add Device menu:

J1939_Manager cannot be added in Machine Expert v2.3 under the CANopen bus node

Product Line

EcoStruxure Machine Expert v2.3

Cause

The CODESYS company as of v3.5 SP17 no longer delivers the J1939 database anymore since because of legal/licensing reasons with SAE International (the parent organization of the J1939 network protocol). And therefore it is why it is also removed from Machine Expert v2.3 as well since our software is based on CODESYS v3.5 SP20.

Resolution

The only recommendation would be to back one version to Machine Expert v2.2.2.

The database was removed by Codesys, which means Schneider Electric cannot deliver the J1939 feature in Machine Expert v2.3 or higher.

The Version v2.2 will still support the J1939 and will remain available to customers.

It may be possible to order the feature from Codesys directly. There exists a CoDeSys paid package for J1939: https://store.codesys.com/en/codesys-j1939-manager-sl.html,

But we cannot guarantee functionality because it would not be an Officially Validated feature by Schneider Electric inside our EcoStruxure Machine Expert product.

If one chooses to try the J1939 package from Codesys, they would need to ask Codesys if it is compatible with the Codesys version specified in Machine Expert.

Schneider Electric cannot guarantee compatibility since this package is not officially validated.

NOTE: The version of Codesys in Machine Expert is found in the Release Notes: EcoStruxure Machine Expert V2.3 - Release Notes | Schneider Electric

Codesys version in the release notes

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)