¿Cómo podemos ayudarte hoy?

Auxiliary Contact Blocks for LC1SK, LP1SK, and LC1SKGC

Issue:

Selection of auxiliary contact blocks for the mini contactors

Product Line:

TeSys™ SK Contactors

Environment:

Contactors and Starters-IEC

Resolution:

LC1SK contactors can be fitted with an add-on block or auxiliary contact block.

LP1SK and LC1SKGC contactors CANNOT accept add-on or auxiliary contact block.

Instantaneous auxiliary contact blocks (Ith: 10 A, Ue: 690 V AC 50/60 Hz)

LA1SK20 - 2 normally open contact block

LA1SK02 - 2 normally close contact block

LA1SK11 - 1 normally open and 1 normally close contact block

Schneider Electric Mexico

Explora más
Rango:
Explora más
Rango: