¿Cómo podemos ayudarte hoy?

Harmony HMIP6 - HMIYP6MPAU Sound Card Line-Out Specifications

Issue

What are the Line-Out specifications of the optional HMIYP6MPAU Sound Card for Harmony P6 iPCs?

Product Line

Harmony P6 Industrial PCs

Environment

Optional PCI slot cards for Industrial PC

Resolution

The HMIYP6MPAU's sound output is a "Line Out" 3.5mm audio output jack with specification of Output Voltage: 1.0 Vrms @10kOhm load.

1.0 Vrms and 10 kOhms impedance is designed for high-impedance loads such as amplifiers/amplified speakers rather than directly driving standard low-impedance (16-32 Ohm) headphones.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)