¿Cómo podemos ayudarte hoy?

QO™ Circuit Breaker Protection FAQs

AFCI, GFCI (standard and HF-rated), & Dual-function circuit breakers for QO™ Load Centers

Learn when to use AFCI, GFCI (standard and HF (high frequency)-rated), & Dual-function circuit breakers for residential applications and light commercial applications including

  • HVAC systems
  • EV chargers
  • pool pumps
  • well pumps
  • general branch circuits

All aligned with NEC 2023 and NEC 2026 requirements where adopted.

Understanding Circuit Protection

What is an AFCI circuit breaker?

Short answer: Protects against electrical fires caused by arcing faults.

Arc Fault Circuit Interrupters (AFCI) detect dangerous arcing conditions caused by damaged wires or loose connections.

What is a GFCI circuit breaker?

Short answer: Helps protect people from electric shock by detecting ground faults.

A Ground Fault Circuit Interrupter (GFCI) breaker trips when it detects ground fault current in the 4-6 mA ranger, per UL 943 Class A requirements, helping protect against shock hazards. A GFCI breaker helps protect the entire circuit, including wiring behind walls.

What is an HF-rated GFCI breaker?

Short answer: A Class A GFCI certified under UL 943 HF to maintain personnel protection when leakage current occurs at frequencies above 60Hz.

HF-rated GFCIs:

  • Are Class A GFCIs certified under UL 943
  • Maintain personnel protection across leakage current at frequencies above 60 Hz
  • Can be used anywhere a standard Class A GFCI is used and provide the same level of ground fault protection
  • Help reduce unwanted tripping caused by high-frequency leakage current from inverter-driven equipment

Common uses:

  • EV chargers
  • Variable-speed HVAC equipment including, heat pumps, mini-splits, and inverter-driven AC condensers
  • Pool & well pumps

Square D™ QO GFCI circuit breakers, now rated for high frequency, are enhanced versions of the existing QO GFCI breakers rather than a separate product.

What is a Dual-function breaker?

Short answer: Combines GFCI + AFCI protection.

Dual-function breakers provide both shock and fire protection in one device and are required in many residential circuits.

What’s the difference between an HF-rated GFCI and a standard GFCI?

Short answer: Both are Class A GFCIs that trip at 4–6 mA of ground fault current. The difference is how they respond to high-frequency leakage current.

Both help protect people from electric shock. The difference is how they respond to high-frequency leakage current from variable-frequency drives and power inverters.

Standard Class A GFCI

  • Can respond to high-frequency leakage current as a ground fault, causing unwanted tripping

HF-rated Class A GFCI

  • Certified under UL 943 HF
  • Designed to trip at variable thresholds based on the frequency of the leakage current found in today's electrified homes and light commercial buildings

Square D QO GFCI circuit breakers

  • Replacing existing standard QO GFCI breakers is not required
  • QO HF-rated GFCI breakers are updated versions of the existing standard GFCI breakers, not a separate product
  • Enhanced to support the higher-frequency loads now common in homes and commercial applications

Which NEC sections apply to HF-rated GFCI circuit breakers?

Short answer: Any section that requires Class A GFCI protection.


HF-rated GFCIs can be used anywhere the NEC requires Class A GFCI protection. Sections where they are most relevant, where adopted, include:

  • 210.8(F) for dwelling unit outdoor outlets, including HVAC equipment
  • 625.54 for receptacles installed for electric vehicle charging
  • 680.21(C) for swimming pool pump motors

Why are HF-rated GFCI circuit breakers recommended for variable-frequency drives and power inverters?

Short answer: These devices produce high-frequency leakage current during normal operation, and HF-rated GFCIs are designed to account for it.


Variable-frequency drives and power inverters produce high-frequency leakage current, which a standard Class A GFCI may interpret as a ground fault. HF-rated Class A GFCIs hold stable during normal operation and still trip on real ground faults.
They can be used on any circuit that requires GFCI protection, whether it's a new home, a service upgrade, or a retrofit.

Can HF-rated GFCI breakers replace existing breakers in Square D QO panels?

Short answer: Yes, but replacing existing standard GFCI breakers is not required.

Square D QO HF-rated 2P GFCI breakers are available in 15–60 A configurations and install as direct replacements in existing QO plug-on neutral load centers. Verify the load center is plug-on neutral before purchasing; pigtail load centers continue to use the pigtail GFCI breaker listed for that load center.

Replacing existing standard GFCI breakers is not required. The QO GFCI breakers that are now rated for high frequency are updated versions of the existing standard GFCI breakers, now enhanced to support the higher-frequency loads common in homes and commercial applications.

Will the QO plug-on neutral HF-rated GFCI breakers work in my existing QO load center?

Short answer: It depends on the load center. Plug-on neutral GFCI breakers require a plug-on neutral load center.


Plug-on neutral QO load centers

  • Manufactured after 2012
  • 12 spaces / 100 A and above

Pigtail neutral QO load centers

  • Older load centers
  • Smaller 2, 4, 6, and 8-space units rated 100 A or less
  • Not compatible with plug-on neutral breakers. Continue using the pigtail GFCI breaker listed for your load center.

Verify that your load center is plug-on neutral before purchasing.

When Do I Need Each Type?


Do I need a GFCI breaker or a GFCI receptacle?

GFCI breaker

  • Protects the entire circuit (including wiring)
  • Ideal for full-circuit protection

GFCI receptacle

  • Protects downstream outlets only
  • More localized protection

Both meet NEC requirements when installed properly.

Do I need an HF-rated GFCI for an EV charger?

Short answer: Recommended

EV charging uses power -conversion electronics that can produce high-frequency leakage current on the circuit. HF-rated GFCIs maintain personnel protection at these frequencies and help reduce unwanted tripping. Verify local requirements with your authority having jurisdiction (AHJ).

Do I need GFCI protection for HVAC equipment?

Short answer: Yes, where adopted (NEC 2026 update).

Starting September 1, 2026, the NEC exception for listed HVAC equipment expires. Under NEC 2026, where adopted, GFCI protection is required for outdoor outlets at dwelling units supplying 208V/240V HVAC equipment rated 60 A or less (50 A or less in jurisdictions still on NEC 2023).

Includes:

  • Heat pumps
  • AC condensers

HF-rated GFCIs are recommended for variable-speed systems to help reduce unwanted tripping from high-frequency leakage current.

Are GFCI requirements the same everywhere?

No.

Requirements vary by:

  • State adoption of NEC versions
  • Local amendments (AHJ rules)

Always verify with your local authority having jurisdiction.

Choosing the Right QO™ Breaker

What’s the difference between QO and Homeline breakers?

QO breakers

  • ¾" per pole
  • Include Visi-Trip indicator
  • Premium performance for residential and commercial applications

Homeline breakers

  • 1" per pole
  • Value-focused option for residential applications and in some instances, light commercial applications

They are not interchangeable. The breakers must match the panel type.

What amperages are available?

  • 1-pole standard: 15–70A
  • 2-pole standard: 15–200A

GFCI:

  • 1-pole: 15–30A
  • 2-pole: 15–60A

What is the interrupting rating (AIC)?

  • Standard QO: 10,000 AIC
  • High interrupting (QO-VH): 22,000 AIC
  • Must meet or exceed available fault current.

Installation & Compatibility

Where does the neutral wire connect?

Plug-on neutral panels

  • No pigtail required

Standard panels

  • Neutral pigtail connects to neutral bar

Can I install QO breakers in a Homeline panel?

No.

Breaker families are not interchangeable due to different bus designs.

Are QO breakers compatible with generators?

Yes.

QO load centers support:

  • Generator interlock kits
  • Transfer switch integration

Troubleshooting GFCI Tripping

Why does my GFCI breaker keep tripping?

Common causes include:

  • Moisture in outdoor boxes
  • Improper or shared neutrals
  • Long wire runs (capacitive effects)
  • LED lighting inrush
  • Variable-speed equipment leakage

Fix:

  • Correct wiring or environmental issues
  • Use HF-rated GFCI for inverter-driven equipment

What do LED indicators mean?

Some QO breakers include diagnostics that indicate:

  • Ground fault
  • Arc fault
  • End-of-life condition

Helps speed up troubleshooting.

Important Code Note

Electrical requirements vary by jurisdiction. Always confirm:

  • NEC version adopted in your area
  • Local amendments

Your local AHJ is the final authority.

Schneider Electric Mexico

Explora más
Producto:
Rango:
Explora más
Producto: