Onze merken

Welkom op de website van Schneider Electric

Welkom op onze website.
		
Waarmee kunnen wij u vandaag helpen?
What is the default IP address of an M340 PLC?
Schneider products equipped with an Ethernet port have a default IP address which is derived from its MAC address (unique identifier assigned by the manufacturer).

If no IP parameters are received from the application when the rotary switch is set to Stored or Clear IP positions, the module is configured at power-up with its default IP address. The default IP address for the module is derived from its hardware MAC address in accordance with a default IP address format

For an M340 PLC, the default IP address format is 84.x.x.x where:

84 = fixed value
x.x.x = the last three fields of the default IP address.
These last three fields are obtained by converting the last three hexadecimal bytes from the MAC address into decimal values.

Example:

The MAC address for an M340 PLC is 000053121AC4.

The conversion of the last three bytes from the MAC address into decimal values gives:

16#12=10#18
16#1A=10#26
16#C4=10#196
Therefore, the default IP address for this M340 PLC is 84.18.26.196.

The default subnetmask: 255.0.0.0.


Notes:

For more information on this subject, refer to the Unity Pro / EcoStruxure Control Expert online help (Deriving IP parameters from a MAC address).

The MAC address is marked on the module.

The method for deriving the IP address of BMXNOE0100 and BMXNOE0110 modules is exactly the same:

Schneider Electric Netherlands

  • Productdocumentatie
  • Software & firmware
  • Productselector
  • Productvervanging
  • Help- en Contact Center
  • Offerte aanvragen?
  • Openingstijden & adressen
  • Vind distributeur
  • Schneider Electric-community
  • Werken bij
  • Bedrijfsprofiel
  • Wangedrag melden
  • Toegankelijkheid
  • Newsroom
  • Investeerders
  • EcoStruxure
  • Vacature zoeken
  • Blog
  • Als eerste op de hoogte nieuws?
  • Dataprivacy
  • Cookiekennisgeving
  • Juridische informatie
  • Change your cookie settings