What is the difference between the REFLEX mode and the POLARISED REFLEX mode on photo-electric sensors?
Note that we no longer sell these devices, this FAQ is for information only.
Both systems comprise a transmitter and receiver (usually within a single-body sensor), and a reflector. The transmitter sends a beam which is bounced back by the reflector and detected by the receiver. An object passing through the beam blocks the reflection and triggers the sensing signal.
REFLEX mode sensors may not be suitable for detecting reflective objects, as a shiny target may bounce the beam back to the sensor in the same way as the reflector. The sensor may not be able to tell the difference between the target and reflector and will therefore fail to detect the object. For maximum effectiveness the targets should be opaque or near opaque and should not be highly reflective in nature. However, the advantage of reflex mode sensors is that they give relatively long sensing distances.
POLARISED REFLEX mode sensors have polarising filters over both the transmitter and receiving sensor. The filters are at 90 deg to each other which means that the receiver cannot see the transmitted beam as it will be blocked by the receiver filter. The reflector turns the polarised light waves through 90 deg so that the receiver can see them. Light bouncing off other objects is not rotated so it will not trigger the sensor. This means that the polarised reflex can be used to detect very reflective surfaces, even mirrors, polished metal and semi transparent materials. However, the sensing distance is shorter than REFLEX.
Gepubliceerd voor: Schneider Electric Netherlands
Hulp nodig?
Selecteer zelf het juiste product
Vind snel en eenvoudig de juiste producten en toebehoren voor uw toepassingen.
Offerte aanvragen
Dien uw aanvraag online in en een expert zal contact met u opnemen.
Verkooppunten
Vind eenvoudig de dichtstbijzijnde distributeur van Schneider Electric op uw locatie.
Help Center
Vind de antwoorden die u nodig heeft via bladeren door veelgestelde vragen over onderwerpen.