Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
What is the part number for an electrical interlock for 9422 disconnect switch?
Issue:
9422 auxiliary contact

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9422 Flange Mounted and Cable Operated

Resolution:
The electrical interlock for a 9422TC1, 9422TC2, or 9422TC3 is 9999R45 for single pole, double throw or you may use a 9999R46 for double pole, double throw.
See table for the rest:

electrical interlocks