Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
Maximum cable length for connection between ION8600 and I/O Expander

Tittle:

Maximum cable length for connection between ION8600 and I/O Expander

Issue:

The cable between ION8600 and I/O Expander must be fixed.

Product Line:

ION8600

Cause:

Extension needed

Resolution

Maximum length between ION8600 and I/O Expander is 45ft (13.7m) (under a controlled test environment).
I/O Expander cables can be extended; however, it will require a specific cable configuration. For example, if you want to extend the connection to a maximum of 16ft you will need to have a cable configuration like the following:

[IO Expander] [A] [B] [A] [ION8600(in breakout panel for example)]

Where:

[A] CBL-8XX0-BOP-I/O BOX: is a 5ft male-male cable to make the IO Expander-ION8600 breakout panel connection
[B] CBL-8X00IOE5FT: is a 6ft male-female cable used to connect an ION Expander to a standard ION8600 with a breakout cable (which is the same as the male connector)

Addendum:

Refer to the most recent version of the Product Part Number Guide to verify the part numbers are up to date.
No official specification exists as this distance was tested under a specific application request. Longer connections may work however nothing beyond 45 has been tested.


Legacy KB System (APS) Data: RESL200178 V1.0, Originally authored by DaMi on 10/06/2009, Last Edited by DaMi on 10/06/2009
Related ranges: ION8600