Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
What communication options are available on the ATV12
Issue:
What communication options are available on the ATV12?

Product Line:
ATV12

Environment:
ATV12

Cause:
Network communications options

Resolution:
The ATV12 only has the modbus communication protocol available.   A third party gateway can be used for other protocol of customer's choice.