Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
Can you feed 230vac into an 480vac Altviar ATV drive to run a 230vac motor?
Issue:
Wha happens if you feed 230vac into an 480vac Altviar ATV drive to run a 230vac motor?

Product Line:
Altivar ATV61, ATV71, ATV312, ATV212 ATV32

Environment:
All

Cause:
They ordered the wrong drive with 480vac they need a 230vac drive can they use the 480vac to run the 230v motor?

Resolution:
No you will need to order the correct drive to match the motor amps, hp and application.