Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
How does the OFS.exe behave when OFS is running as a Windows service?
Issue
How does the OFS.exe behave when OFS is running as a Windows service?

Product Line
OPC Factory Server (OFS)

Environment
Windows 10 version 1902, OFS v3.62

Resolution
When running as a Windows service the 'Ofs.exe' still runs as a process alongside with the OFService service.  The OFService acts as a OFS COM client.