Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
What is the significance of the 'C' or 'B' suffix on an ATV320 drive part number?
Issue:
What is the significance of the 'C' or 'B' suffix on an ATV320 drive part number?

Product Line:
Altivar 320

Environment:
All

Cause:
N/A

Resolution:
B suffix is a bookshelf version of the ATV320 drive.  This is a slim style version.
C suffix is a compact version of the ATV320 drive.  This is a more cube-shaped drive.