Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
PME 8.2 Vista crashes when trying to modify the scale on a horizontal or vertical bar views of a numeric object

Issue
In order to modify the scale on a numeric object with a  horizontal or vertical bar view in Vista, one must go to the Object Configuration and right click on the numbers in the preview.  In PME 8.2, there is an issue where this causes Vista to crash giving the following error message.

Vista error

Product Line
Power Monitoring Expert 8.2

Cause
This has been logged as a bug in PME 8.2 and has been resolved for PME 9.0 and up.

Resolution
The workaround is to only right click the tick marks in between the numbers instead of the numbers themselves.  That way, it will work as previous PME versions and give you the ability to change the horizontal or vertical axis depending on which style was selected.