Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
How can it be verified the motor is running through the shorting contactor and not the ATS48?
Issue:
Validate motor is running through the shorting contactor, not the soft starter.

Product Line:
ATS48

Environment:
All serial numbers

Cause:
Testing the contactor

Resolution:
Verify the r2A and r2C is closed.
Measure motor current on the load side of the shorting contactor.