Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
Is it possible to use master-slave in torque on ATV320?
Torque sharing cannot be used with ATV320 drives.
To be able to manage torque sharing via analog sgnal, the slave must work in torque control mode.
Unfrotunately ATV320 cannot work in torque control because there is no SVCI (sensorless vector control in torque).
Alternative is
- ATV71 (master slave via analog signal)
- ATV930 (MS via analog or better via multidrive link)
- ATV340...E (MS via MDL)