Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
What Lonworks communication options are available on the ATV630 and ATV930 Process drives?
Issue:
Is Lonworks available on the ATV630 and ATV930 drives?

Product Line:
ATV630 and ATV930 drives.

Environment:
All

Cause:
Available options

Resolution:
The ATV630 and ATV930 drives do not currently have an option for Lonworks.  If you need to use Lonworks on the ATV630 and ATV930 drives you need to add a third party gateway.