Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
Can the ATV630 maintain a constant pressure using Sensorless flow estimation ?
Issue:
Can the ATV630 drive be configured to maintain a constant pressure, using the Sensorless flow estimation function?

Product Line:
ATV630

Environment:
All serial numbers

Cause:
No external PI control

Resolution:
No, it is not possible to maintain constant pressure control with Sensorless Flow Estimation.