Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
To do what, is used the mechanical thermostat NSYCCOTHO with blue button?
To cool the inside of an enclosure by blowing fresh outside air into the enclosure using a fan.
This mechanical thermostat has an open contact.
When the temperature inside the enclosure exceeds the set point, the contact closes and a fan starts.
This implies that the outside air is colder than the set point T °.