Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
PME2020-Parameters not visible in Breaker Configuration tool

Issue
In PME2020 Chinese version of Breaker Configuration Tool, we can see the issue, when you choose the -- Is existing breaker device?
It can’t show all the parameters in this section:
aa

Resolution:
This Issue already fixed in PME2020 CU3.

a

After installed CU3, when run the Breaker Configuration Tool, now we can see the parameters:
a