Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
Harmony P6: Application Launcher including 3 touch modes
Goals and Symptoms
The Launcher of Harmony P6 is a utility that you can set up to start programs and settings. It allows to manage the settings for convenient touch-screen operations.
The goal of this resolution is to get familiar with the Application Launcher
Causes and Fixes
Here is the video to show the functions of the Application Launcher