Merkene våre

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
PowerChute Network Shutdown error when setting password

Issue:
When setting the password for PowerChute Network Shutdown version 4.4 or 4.4.1, the web UI reports "This field contains unsupported characters." or "Unsupported character set." when the password contains an arrow < > character.

Product Line:
PowerChute Network Shutdown versions 4.4 and 4.4.1

Environment:
All supported OS

Cause:
Misinterpretation of the characters < >

Solution:
Set the password with characters other than an arrow. If the < > characters are required, follow the instructions in FAQ FA159758 to reset the password using the pcnsconfig.ini file.