Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can the PDL356PB2MBTZ-VW be configured as a time delay switch?

When paired with a hub, functions like time delay switching with the wiser switches are achieved via automations. An automation can be configured to activate a delay timer and off function following the switch being turned on.

Below is an example of an automation configuration where a wiser switch controlling some hallway lights will automatically turn off 20 seconds after they are turned on.

Image of the automation window from the Wiser by SE app, showing condition 1/10 being Hallway Switch: On. also showing Actions 2/80 being Delay: 20 seconds, Hallway switch:off. Effective period: All-Day

Schneider Electric New Zealand

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software and Firmware
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Where to Buy?
  • Office Locations
  • Schneider Electric, PDL & APC Phone: 0800 741 303
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
  • Conditions of Sale
  • Change your cookie settings