Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Resolve "No Instance available to allocate %TMA" Error from Machine Expert Basic V1.3

Issue:

This Error "No Instance available to allocate %TMA" sometimes happens when trying to compile an uploaded project using Machine Expert Basic V1.3

Resolution:

1. This is a bug in ESME-Basic V1.3. and is fixed in ESME-Basic V1.4

2. If you are still using ESME-Basic V1.3, please follow below solution:

After uploading the project, logout and go to the Programming tab >> Tools >> Software Objects >> Timers:

In the Timer properties window, switch the Allocation option from Automatic to Manual and then from Manual to Automatic and click Apply. Then compile and login back.

solution image

Schneider Electric New Zealand

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software and Firmware
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Where to Buy?
  • Office Locations
  • Schneider Electric, PDL & APC Phone: 0800 741 303
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
  • Conditions of Sale
  • Change your cookie settings