As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
Can a remote speed signal be wired to an ATV212 S-Flex drive?
Issue:
Remote speed signal wiring on an ATV212 S-Flex drive

Product Line:
Altivar ATV212, SFlex 212

Environment:
All

Cause:
Customer didn't know how the speed signal was wired in the ATV212 S-Flex.

Resolution:
Yes, a 0-10Vdc, 0-20mA, or a 4-20mA analog signal can be wired to the VIA Terminal on the drive.
Only a 0-10v or PTC motor thermal probe can be used with terminal VIB.

NOTE: Dipswitches are used to set these terminals for Voltage, Current or PTC.