Pesquisar nas perguntas frequentes (FAQ)
How do you set up the ATV58 drive for local control with keypad?
Issue:
Local control set up with ATV58 keypad.
Product line:
Altivar ATV58
Local control set up with ATV58 keypad.
Product line:
Altivar ATV58
Environment:
All models, all serial numbers
All models, all serial numbers
Cause:
Setting up the ATV58 to be controlled with the remote keypad display.
Resolution: Setting up the ATV58 to be controlled with the remote keypad display.
Menu 4 set LCC to yes
Publicado para:Schneider Electric Portugal
Explorar mais
Explorar mais