Pesquisar nas perguntas frequentes (FAQ)
To identify the voltage limits or Tolerence for the ZB4-BW0** transformer pilot light bodies? Can the ZB4BW055 operate upto 440V?
Goals and Symptoms
To identify the voltage limits or Tolerence for the ZB4-BW0** transformer pilot light bodies? Can the ZB4BW055 operate upto 440V?
Facts and Changes
ZB4
ZB4BW
Transformer
Voltage Limits
Causes and Fixes
The voltage limit is +/- 10%.
=> Mini = 360V~ - Maxi = 440V~.
Legacy KB System (APS) Data: RESL160826 V1.0, Originally authored by LaBe on 09/19/2007, Last Edited by LaBe on 09/19/2007
Related ranges: Harmony style 4
Publicado para:Schneider Electric Portugal
Explorar mais
Gama:
Explorar mais
Gama: