As nossas marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como o podemos ajudar hoje?
What is the difference between a Unity .STU project and an .XEF project?

An .STU file is a project created in Unity Pro.
An .XEF project is a Unity Pro application exchange file. It is a project that has been exported from Unity Pro.
NOTE: Any file extension beginning with an 'X' indicates the XML format (extensible markup language).


Legacy KB System (APS) Data: RESL162229 V1.0, Originally authored by on , Last Edited by on
Related ranges: Unity Pro