Pesquisar nas perguntas frequentes (FAQ)
What are the differences between Modbus Plus cables 990NAD219xx, 990NAD218xx and 990NAD211xx?
Goals and Symptoms:
What are the differences between Modbus Plus cables 990NAD219xx, 990NAD218xx and 990NAD211xx?
Causes and Fixes:
The following tables list the available Modbus Plus cables and accessories and the PLC's with which they connect.
Cables and Accessories:
Note::
The AS-MBKT-085 and AS-MBKT-185 connectors can be used with all of the PRODUCTS that support Modbus Plus with any of the 490NAA Modbus Plus cables listed above.
Publicado para:Schneider Electric Portugal
Explorar mais
Gama:
Explorar mais
Gama: