Como o podemos ajudar hoje?

How far away from the Circuit Monitor Series 2000 can I mount the RTM (ride-through module)?

Issue:

Customer would like to mount the RTM physically and needs to know the maximum distance allowed from the CM2000 Series.

Product Line:

CM2150

CM2250

CM2350

CM2450

Environment:

Installation of a Ride-Through Module on a CM2000 Series Meter

Cause:

The RTM was installed in a location that did not comply with the required mounting distance from the Circuit Monitor.

Resolution:

The RTM can be mounted on the back of the Circuit Monitor or can be mounted remotely, as long as it is mounted within 10 feet of the Circuit Monitor.