Pesquisar nas perguntas frequentes (FAQ)
What is the part number for a CT shorting terminal block?
Issue What is the part number for a CT shorting terminal block? Product Line Power Meter Accessories Environment All meter applications with current over 5 Amps which require Current Transformers. Cause Information needed on shorting terminal blocks Resolution For a 4-pole shorting block it is 3090TB4 and for the 6-pole it is 3090TB6 UPDATE Year 2014 Going forward any 3090TB4 or 3090TB6 Shorting Terminal Block ordered will be Cooper Bussmann branded and not Marathon branded. 3090TB6 = Cooper Bussman model KUXSC6S2644 3090TB4 = Cooper Bussman model KUXSC4S2644 *Cutsheet attached below* The shorting screws for the 3090TB4 and 3090TB6 CT shorting blocks can be purchased from "Marathon Special PRODUCTS" The part number for the shorting screws is "9616901". Both the 4-pole and 6-pole CT shorting blocks require a quantity of 4 of the provided screws part number. Internal PMO/PMC All content © 1992-2007 Schneider Electric | |
Legacy KB System (APS) Data: RESL185215 V2.0