Pesquisar nas perguntas frequentes (FAQ)
Job [ION EEM APP] IONDatabaseLoader Data reported: Unable to open Step output file.
Goals and Symptoms
EEM 4.0 R2 with CU#3
SQL 2008 R2 64 bit Enterprise Edition
[ION EEM APP] IONDatabaseLoader Data" SQL task was generating an error:
Date 7/25/2013 12:00:27 PM
Log SQL Server Agent (Current - 7/25/2013 12:00:00 PM)
Message
[136] Job [ION EEM APP] IONDatabaseLoader Data reported: Unable to open Step output file.
Causes and Fixes
The following steps resolve the issue:
1) Identify failed job and open the job in SQL Server agent.
2) Select the steps.
3) Select the failed step.
4) Edit the failed step, it will open new window.
5) Select the Advanced option in the left side window.
6) Right side of the window Output file box change the output file path.
7) Ran the job, job ran successfully.