How to configure the ION Real Time Data Service in ION/SPM/PME to use a different port
Issue
How to configure the ION Real Time Data Service in ION/SPM/PME to use a different port
Product Line
ION Enterprise 6.0.x
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024
Environment
ION Real-Time Data Service Configuration
Cause
A new port may be desired for the ION Real-Time Data Service
Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*
1. Open SQL Server Management Studio
2. Expand out the ION_Network database and then expand the Tables.
3. Find the table named "dbo.Registry". Right-click on the table and select "Edit Top 200 Rows"
4. In that table, there is a field named "Remoting.IONServices.Port" and its default value is NULL. Specify a port # in this field and restart the Real Time Data Service to use this port for its TCP comms.
Disclaimer: There are limitations on the values you can enter in this field. Values that are lower than 1024 or higher than 49151 may cause IONServices to not start up.