Pesquisar nas perguntas frequentes (FAQ)
PowerLogic CM2000 (CM2) Firmware version 17.011 for use with DLF3000 and DLF101 (fix for rapid energy accumulation on previous versions of firmware)
Product Line
CM2000
Environment
Firmware
Resolution
The attached .zip file contains a .fw file for DLF3000 version 3.0, and a .sys and .hex file for DLF101, if needed.
Note: This is the most up to date version of the firmware for a CM2 series meter.
Publicado para:Schneider Electric Portugal
Anexo(s)
Explorar mais
Gama:
Explorar mais
Gama: